Dear Sir,
According to the datasheet description of Integrated 2×2 Cross-Point
A non-disruptive on-chip eye monitor and a PRBS generator and checker is available for in-system diagnostics
Can PRBS generator to check the below 2 loop? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
According to the datasheet description of Integrated 2×2 Cross-Point
A non-disruptive on-chip eye monitor and a PRBS generator and checker is available for in-system diagnostics
Can PRBS generator to check the below 2 loop? thanks.
Hi Lucifer,
You can do from RX0 to TX1 and RX1 to TX0. Device does not support loop back from RX0 to RX1 or TX0 to TX1.
Regards,,nasser
thanks sir.
Since datasheet doesn't show the layout rule, may provide me layout guide as well? thanks.
Hi Lucifer,
Layout guideline is part of the application section of the data sheet. Please refer to this section.
Additionally, DS250DF230EVM pcb layout is part of the design documents and you can review this Allegro pcb layout as well.
RRegards,,nasser