This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10002: The Serdes register setting of TLK10002

Part Number: TLK10002

Hi team,

My customer are using the TLK10002 in their system.

They found that their power supply 1V may have 80mVp-p, 140kHz ripple that cause the bit error in serdes.

And after they change the serdes setting(as below), the bit error has improved 

The HS_CDRFMULT from 01 = Second order. 1x mode to 02 = Second order. 2x mode

The HS_CDRTHR from 11 = Thirty two vote threshold to 10 = Sixteen vote threshold],

So the customer want to know the effect of their change, will this cause iincrease of the power consumption or if there are some other side effect of the change?

Lacey

Thanks a lot!