This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: RGMII Series Termination Details and Voltage Domain

Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869

On page 14 of the datasheet the following information can be found regarding series termination of the RGMII port:

This would imply that the series termination resistors are only on the RX pins of the port.  Are they also included in the TX pins or will I need to add them external to the chip?

Also, what is the voltage domain of the RGMII signals?  More specifically if I change the supply voltage on VDDIO from 2.5V to 3.3V will it impact the signaling levels of the RGMII interface?  I plan to interface the RGMII of the DP83869HM to the RGMI port on another device where the voltage domain is 2.5V.  Thanks