Part Number: AM26LS32AC
Other Parts Discussed in Thread: AM26LS31
Team,
Two manufacturers made a subassembly I am testing. One used the correct 26ls31 driver, and the other used two 54S240 inverters (one input is inverted by 54LS04). The subassembly that receives this circuit has a 26LS32DM , with 6.8 to 9k input resistance (calculated or inferred from other tests). I am told this correctly generates the expected outputs for both manufacturers at the box and system level. I used the AM26LS32 in test receiving circuit, which has input resistance of 12 to 15K. It only passes the manufacturer that used the 26ls31 driver.
Page 15 has the equivalent circuit for AM26LS32AC. http://www.ti.com/lit/ds/symlink/am26ls32ac.pdf
The test circuit has the normal 1k serial terminations, which can be removed easily. The 26ls31 or 54S240 do not have any serial termination resistors in their respective subassemblies. Is getting an IC with the lower input resistance the only option? Is there an issue with PCB footprint dimensions between the commercial AM26LS32 and the mil qualified parts with the lower input resistance?
Thank you.