Part Number: TPS65983B
Hi there,
We are currently building Thunderbolt3 FW (Titan Ridge - Tapex Creek TI83) and need to include PD FW in Thunderbolt EEPROM. Our application only use Thunderbolt3 to PCIe. There are two Intel JHL7440 ICs and each JHL7440 has two PDs (one downstream and one upstream). The downstream will be depopulated since there will be no cascade downstream device. This is our EVT build and we keep it just in case. We will not use DP, USB, power charging from upstream or to downstream device. No USB2.0 connection from PD to JHL7440. The power is self power. The PP_5V is from our PCB 5V VR and it can support 2.5W per each PD. The VBUS is connected to USB C (Thunderbolt 3) connector. The schematic had been checked by your team and confirmed no problem. Some questions need your help.
1. I requested the PD FW and got TPS65983_FW_6.61_Windows & TPS65983_FW_4.61_Windows from your side. What is the difference between these two? I'm using TPS65983_FW_6.61_Windows for now.
2. I attached the pjc file and need your help to check if anything need to be modified.