hi team,
we want to check the Vo common mode voltage range of the device, whether it has connection with the Vod configuration? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi team,
we want to check the Vo common mode voltage range of the device, whether it has connection with the Vod configuration? Thanks.
Hi Frank,
There is a relationship between VOD and VOC. As VOD increases and the VOC decreases, they trend in opposite directions. The typical value for VOC is ~1.1V, however this value varies widely and can be as low as 0.6V or as high as 1.5V.
The device VDD also plays a big role in the output VOC level. Device VDD and output VOC will trend in the same direction. Increases in VDD will bring similar changes in VOC.
Regards,
Lee