Part Number: SN75DPHY440SS
Hi Sir,
Could our re-timer's MIPI Lane be changed or swap casually?
For example, Lane0/Lane1 swap & Lane2/Lane3 swap.
If so, could you please guide us how to do that?
Thanks,
George
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75DPHY440SS
Hi Sir,
Could our re-timer's MIPI Lane be changed or swap casually?
For example, Lane0/Lane1 swap & Lane2/Lane3 swap.
If so, could you please guide us how to do that?
Thanks,
George
George
It depends on whether this is a DSI or a CSI-2 application.
For DSI
One of the four lanes is used for back channel communications between GPU and DSI panel. DPHY440’s lane 0 is the only lane that supports the back channel. For this reason, DPHY440 lane 0 must always be connected to lane 0 of GPU and panel.
For CSI-2
The DPHY440 supports 4 CSI-2 DPHY lanes plus a clock. Unlike DSI, CSI-2 does not have a back channel path. Because of this, there is no requirement on lane ordering. Because there is no lane ordering requirement, there are more combinations which can be implemented. All possible combinations are supported by the DPHY440. For all CSI-2 implementations, the polarity must be maintained between the CSI-2 Source and CSI-2 Sink. The DPHY440 does not support polarity inversion.
Thanks
David