This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65CML100: 1.2V CML Driver

Part Number: SN65CML100
Other Parts Discussed in Thread: DS10BR150

I would like to use this part to drive 1.2V CML line.  Based on the data sheet and app note, i plan on using two 50 Ohm resistors as bias generators at the output of the chip, connected to 1.2VDC.  Additionally, there will be two 50 ohm resistors terminating the line at the receiver, also connected to 1.2VDC.

The LVDS input will be terminated with 100 Ohms across the input lines.

Any thoughts on using this part as a 1.2V CML driver?

Thanks.

Frank