Part Number: TLK10232
Our customer is asking us the Communication detection.
Could you kindly advice us the following two question?
Phenomenon
- CPU does not detect 10Gb ethernet inactivity of ChB even if 10Gb ethernet line is disconnected. See “10Gb Ethernet circuit.pdf”.
- This phenomenon occurs when registers are not optimized and disappears by optimization. See “Register Set.pdf”.
- See “Channel Status1.pdf”. This table shows TLK10232 register “CHANNEL_STATUS_1” when the phenomenon occurs.
Questions
- Is there any possibility for TLK10232 to indicates “CHANNEL_STATUS_1” register status above in such a case?
- What kind of XAUI output waveform can be observed when the phenomenon occurs?
Thank you & Best Regards,10Gb Ethernet circuit.pdfChannel Status1.pdfRegister Set.pdf