Hi Team,
I have a question about understanding of the absolute rating in the datasheet. Please see below screen shot.
Per spec, CC pin's voltage rating is VDD+0.3V,
Question: Does it means CC pin's voltage rating must be lower than VDD+0.3V?
For example, in the application of battery, VDD is 3.7V, so the voltage rating is 4.0V in this case? If not, can CC pin supports 6.3V? Thanks!
-Wenhao