This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3415: PCIe switch from 16 lanes to two ch. of 8 lanes

Part Number: HD3SS3415

Hello team,

Could you please advise if TI has the following solution.

My customer is looking for a PCIe switch, GEN3. (Max. bit rate, 8Gbps)

The host (SOM) is connected via 16 lanes to 2 FPGA’s are connected, each via 8 lanes bus.(See block diagram below).

Thanks in advance

Best regards,

Shai