This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8040: Type-C hub with display port support

Part Number: TUSB8040

Team,

One customer, they are going to make the notebook, and it will have two type-c port. They want both of them are full function, could support USB devices and also display port. So they are looking for full function type C hub.

They said, ideally, if two monitor connected to the type c ports, if they can be identified as monitor 2 and monitor 3, display diff information, it will be best they want; but if it does not work, they can accept two monitors display the same thing.

What is our suggestion on this kind of function? And experience? Could Win 10 display driver support this?

Best REgards,

Peter Wei