This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB213: Problem on cascade of TUSB213

Part Number: TUSB213


I have a project to support long trace for a USB OTG deivce.I place one TUSB213 near CPU,and the otherone near connector,which level (DC&AC Boost) is better for this case. I must to use the both of HOST and SLAVE mode of the CPU.

  • Hi,

    What exactly is the failure you are seeing? What is the total trace length from CPU to connector? Where are your TUSB213 placed along the trace? TUSB213 is bi-directional, CPU mode should not impact function of TUSB213.

  • Hi,

    Is there any more support needed for this issue? If so please reply with any relevant details so that I can further assist you. For now I will be marking this thread as "TI Thinks Resolved". If you have resolved your issue, please post the solution to the original problem/post for others with similar issues.