This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIC12400-Q1: would TIC10024-Q1 or TIC12400-Q1 support applications with 24V battery?

Part Number: TIC12400-Q1
Other Parts Discussed in Thread: TIC10024-Q1

E2E,

I'm using a 24V battery, and even if TIC datasheet mentions a 35V recommended power supply (40V max. abs), it is noted that this voltages were tested at load dump for a 12V nominal battery, so, would TIC10024-Q1 or TIC12400-Q1 support applications with 24V battery?

Thank you,

Adam