This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS10BR150: Unused pin and output voltage with external termination resister

Part Number: DS10BR150
Other Parts Discussed in Thread: DS25BR110, DS25BR120, , DS25BR100, DS25BR150

Hi

 

Our customer is considering the one of the below and therefore would like to use same layout.

 

DS25BR110

DS25BR120

DS10BR150  

DS25BR100  

DS25BR150  

 

 

1pin and 4pin of DS10BR150 / DS25BR150 are NC.

Are there any issues if these pins were connected to GND or VCC ?

 

All the above 5 products could output 350 mV with external 100 ohm termination resister ?

Our customer assume it would be OK because the datasheet describe differential output voltage is 350 mV with test condition RL = 100 ohm.

Thank you and best regards,

Michiaki