Team,
The data sheet for the SN55LVCP22-SP only specifies a minimum frequency of 1 GHz. What is the max operational frequency? Can it run at 3.125 GHz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
The data sheet for the SN55LVCP22-SP only specifies a minimum frequency of 1 GHz. What is the max operational frequency? Can it run at 3.125 GHz?
Hi Michael,
The maximum operating frequency depends on the rise time. The typical rise time given in the datasheet only allows for a maximum operating frequency of around 1.25 GHz. 3.125 GHz is too fast for this part.
Regards,
I.K.