Hi experts,
I want to use UB960 to deserialize the camera data from DS90UB913Q, UB913 run in RAW12 HF mode. Could you please provids the register configuration of UB960 through I2C to compatible with UB913?
Best Regard,
Hutian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
I want to use UB960 to deserialize the camera data from DS90UB913Q, UB913 run in RAW12 HF mode. Could you please provids the register configuration of UB960 through I2C to compatible with UB913?
Best Regard,
Hutian
Hello Hutian,
960 is only qualified for compatibility with 913A, not 913Q. Can you confirm if 913A is the device you are using?
Best Regards,
Casey
Hi Casey,
My mistake for the type of the UB913, we are using DS90UB913A not 913Q. Could you please provide the configuration for ub960 to compatible with ub913A?
Thanks,
Hutian
Hello Hutian,
All that is needed to pair 960 with 913A is to set the proper MODE pin strapping. In this case make sure that the 960 MODE pin is strapped for RAW12 HF and connect the 960 to the 913A module. They should link automatically.
Best Regards,
Casey
Hi Casey,
We are using "ADAS Sensor Fusion BoardC" and the MODE pin is set to setting to compatible with UB953, hence we need to setting in SW level.
Whether is it possible for us to let MODE pin setitng in UB953 mode, but configure register to compatible with UB913?
Thanks,
Hutian
Hello Hutian,
Yes the MODE setting can be overridden with registers. Please use register 0x4C to select which RX ports you want to change and then use register 0x6D[1:0] to select the RAW 12 HF mode.
Best Regards,
Casey
Hi Casey,
Thank you for your support, i have already get the Sensor data form UB960 with seriliser UB913A.
Thanks,
Hutian