Other Parts Discussed in Thread: ALP, USB2ANY
Hello,
I'm using 954 evb and a camera with 953.
The I2C is generated from another computer connected to 954 evb and from there to the camera.
The samples are 1M I2C write messages, 954 evb above and 953 below.
There is a 50us from the start of the transaction until the ACK of the 954 (or 37us from the end the "real" ack at the camera to the ACK of the 954).
How this 37us can be shortened? (tried auto ack, disabled local ack and it didn't help)