Part Number: DS26C31MQML
Other Parts Discussed in Thread: SN65HVD78,
Hi, I'm daejin
I am using the part for 422 communication.
the 422 communication test result used the part is success.
but, unfortunately after test I found an odd problem during to impedance check.
If the part is nominal, impedance between Pin 2 and Pin 8(GND) is greater than 1 Mega ohm.
but, when I measured the impedance, the measured value is approximately 75 ohm and Pin 3 to Pin 8 is 6.8 k ohm.
Actually, 422 communication was fully succeeded but, after test impedance value was odd.
I'm wondering why this problem occurred.
could you help me about this issue?
thank you in advanced
daejin.