This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Port 0 Source/Sink GPIO event unexpected behavior

Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, BQ25713,

Hi,

We are seeing strange behavior when configuring the TPS65987 profile to assert GPIO20 using "Port 0 Source Sink Event" when it is Sink. This is the way we have it set up.

There are 2 issues,

1) instead of asserting and stay high, we are seeing a toggle instead, the lines goes high for several milliseconds and then goes back low.

2) When we use same even, simultaneously, with another GPIO (GPIO1 in our case), the GPIO20 does not even change states.

Is this expected behaviour? If not could you please help understand the issue?

Thanks,

Ilya