This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS31: Regd IOH and IOL value of the device

Part Number: SN65LVDS31

Hi,

1) The absolute maximum rating of IOH and IOL is not mentioned in the datasheet. Is it same as the output short circuit current of the device? 

2) Equation for calculating the max operating frequency from the rise time?

  • Hi Akash,

    1) It's an LVDS driver so IOH/IOL are not relevant specs

    2) I'm not sure what the equation used for this device was but typically you can use:

    Bandwidth[Gbps] = 0.35 / rise time [ns]

    to estimate the max frequency.

    Regards,

    I.K.