This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer is applying HDMI HDCP certification and see below error message,
1.ERROR(SP02): Bstatus: HDMI_MODE bit was one
2. ERROR(SP05): All five bytes of KSV FIFO was not zero
3. ERROR(S102X): Bcaps: REPEATER bit was 1,
Is there any required setting on DS90UH949 for HDMI HDCP certification ?
Do the MCU need to do any action on DS90UH949 in react to HDCP authorization ?
Below are the DS90UH949 register setting, is there any setting missed?
[REGISTERS] Device = ALP Nano 1 - DS90UH940, Connector 1 Comments = "14" Date = 09/22/2020 Time = 17:02:01 Reg = 0,0x0000,0x58 Reg = 0,0x0001,0x04 Reg = 0,0x0002,0x00 Reg = 0,0x0003,0xF0 Reg = 0,0x0004,0xFE Reg = 0,0x0005,0x1E Reg = 0,0x0006,0x00 Reg = 0,0x0007,0x24 Reg = 0,0x0008,0x00 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0x00 Reg = 0,0x000B,0x00 Reg = 0,0x000C,0x00 Reg = 0,0x000D,0x00 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x00 Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x00 Reg = 0,0x0016,0x00 Reg = 0,0x0017,0x00 Reg = 0,0x0018,0x00 Reg = 0,0x0019,0x01 Reg = 0,0x001A,0x00 Reg = 0,0x001B,0x00 Reg = 0,0x001C,0x33 Reg = 0,0x001D,0x40 Reg = 0,0x001E,0x00 Reg = 0,0x001F,0x00 Reg = 0,0x0020,0x00 Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x00 Reg = 0,0x0023,0x20 Reg = 0,0x0024,0x08 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x83 Reg = 0,0x0027,0x84 Reg = 0,0x0028,0x00 Reg = 0,0x0029,0x00 Reg = 0,0x002A,0x00 Reg = 0,0x002B,0x00 Reg = 0,0x002C,0x00 Reg = 0,0x002D,0x00 Reg = 0,0x002E,0x00 Reg = 0,0x002F,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x00 Reg = 0,0x0033,0x00 Reg = 0,0x0034,0x00 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x88 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x2F Reg = 0,0x003C,0x20 Reg = 0,0x003D,0xC0 Reg = 0,0x003E,0x23 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x00 Reg = 0,0x0041,0x03 Reg = 0,0x0042,0x03 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x60 Reg = 0,0x0045,0x88 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x0F Reg = 0,0x0049,0x00 Reg = 0,0x004A,0x00 Reg = 0,0x004B,0x08 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x63 Reg = 0,0x004F,0x00 Reg = 0,0x0050,0x00 Reg = 0,0x0051,0x10 Reg = 0,0x0052,0x00 Reg = 0,0x0053,0x01 Reg = 0,0x0054,0x80 Reg = 0,0x0055,0x00 Reg = 0,0x0056,0x00 Reg = 0,0x0057,0x00 Reg = 0,0x0059,0x7F Reg = 0,0x005A,0x20 Reg = 0,0x005B,0x20 Reg = 0,0x005C,0x00 Reg = 0,0x005D,0x00 Reg = 0,0x005F,0x00 Reg = 0,0x0060,0x00 Reg = 0,0x0061,0x00 Reg = 0,0x0062,0x00 Reg = 0,0x0063,0x00 Reg = 0,0x0064,0x10 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006A,0x00 Reg = 0,0x006B,0x00 Reg = 0,0x006C,0x00 Reg = 0,0x006D,0x00 Reg = 0,0x006E,0x00 Reg = 0,0x006F,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x07 Reg = 0,0x0074,0x07 Reg = 0,0x0075,0x08 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x18 Reg = 0,0x007C,0x02 Reg = 0,0x0080,0x27 Reg = 0,0x0081,0xE5 Reg = 0,0x0082,0x00 Reg = 0,0x0083,0x14 Reg = 0,0x0084,0x7C Reg = 0,0x0090,0x9E Reg = 0,0x0091,0xED Reg = 0,0x0092,0x4F Reg = 0,0x0093,0x06 Reg = 0,0x0094,0x18 Reg = 0,0x0098,0x8C Reg = 0,0x0099,0x8D Reg = 0,0x009A,0x04 Reg = 0,0x009B,0xED Reg = 0,0x009C,0xAA Reg = 0,0x009D,0x17 Reg = 0,0x009E,0x07 Reg = 0,0x009F,0x5C Reg = 0,0x00A1,0x00 Reg = 0,0x00A2,0x8C Reg = 0,0x00C0,0x00 Reg = 0,0x00C1,0x00 Reg = 0,0x00C4,0x01 Reg = 0,0x00C5,0x00 Reg = 0,0x00C8,0xC0 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00E0,0x00 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0x00 Reg = 0,0x00E3,0x00 Reg = 0,0x00E8,0x01 Reg = 0,0x00E9,0x00 Reg = 0,0x00EA,0x00 Reg = 0,0x00F0,0x5F Reg = 0,0x00F1,0x55 Reg = 0,0x00F2,0x48 Reg = 0,0x00F3,0x39 Reg = 0,0x00F4,0x34 Reg = 0,0x00F5,0x30 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
Hi,
What are you setting register 0xC3 to?
Regards,
Michael W.