This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB214-Q1: Should Redrivers be used as a pair for long distances?

Part Number: TUSB214-Q1
Other Parts Discussed in Thread: TUSB212-Q1, TUSB216

We have an application that will be transmitting USB 2.0 over ~15ft and also in the presence of some power supply and motor noise (though the twisted pair with the USB signals will be shielded). To mitigate potential signal integrity issues, we are looking at using the TUSB214-Q1. However, my question is whether it is a good idea to actually use two of these - one at the host and another at the device end?

Thank you.