Part Number: TCA9535
Hi Team,
I have questions about TCA9535 so could you help?
[Question 1]
when we tied unused pins to Vcc or GND directly, are there any concern?
[Question 2]
regarding abso max spec, Iol continuous output low current is 50mA so we have to follow this current level.
question here is TCA9535 Icc continuous current through GND is -250mA so does it mean total Iols + leak current must be less than 250mA?
[Question 3]
is it ok to tie every unused pins with single pull up resistor?
Regards,
Kai