Part Number: TCA9517
Other Parts Discussed in Thread: TMP175, TCA9546A
hello
I try to measure temperature using TI device (TMP175).
There is only one bus which is communicating with I2C, but I need 26EA device(TMP175) in parallel.
I had two concern, First I need device which have many slave address . Second I need to reduce bus capacitance. (limit 400pf in I2C )
That's why I chose TMP175 and I decide to add buffer. But I don't know what i have to choose yet.
I attached my block diagram. Is there any problem ? Could you plz recommend any solution and you can choose buffer ( TI's device)
Board 1 is made already . I try to design board 2 now. 3.3V power is short in board 2 . So I have to use TCA9517 to shift to 5V.
Thank you.