Part Number: TCA9535
Hi Danny-san
From following session.

Customer have additional question.
Which is correct?
1: "SCL/SDA don't have any path to Vcc".
or
2: "SCL/SDA have the path to Vcc, but IC can accept leakage current for IC damage"
Thanks
Muk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9535
Hi Danny-san
From following session.

Customer have additional question.
Which is correct?
1: "SCL/SDA don't have any path to Vcc".
or
2: "SCL/SDA have the path to Vcc, but IC can accept leakage current for IC damage"
Thanks
Muk
Muk-san,
Good to hear from you, and thanks for following up!
The device should remain high-impedance when unpowered (VCC = 0) even if there is a pull-up or pull-down to a power/GND rail on SCL/SDA. You shouldn’t expect to see any high leakage current unless the SCL/SDA pins are pulled below GND or above VCC, in which case some body diodes may begin reverse breakdown or it may start to power an ESD cell.
Best,
Danny