Hi Protection team,
I'm looking for ESD and Vbus-CC short protection IC and here is requirement for USB.
[Requirement]
USB data: USB2.0
USB cable: USB type-C cable but only support USB2.0 communication(no SS).
Power: 5V/500mA
need DRP so use TUSB320LAI as CC control
[ESD protection]
I pick up TPD6E05U06 as ESD protection.
- Vbus, CC1/2 and DP/DM ESD protection: TPD6E05U06
-
[Vbus-CC short protection]
First I pick up TPD6S300A but it's CC clamp voltage is 8V_typ.
In this system, there is no PD requirement so Vbus voltage is 5V.
TUSB320LAI CC abso max voltage is 6V so 8V is higher than CC abso max.
[Question]
I picked up TPD6E05U06 as ESD protection but are there any other 1 chip solution supporting Vbus, CC1/2 and DP/DM ESD protection?
Are there any good protection devices supporting Vbus-CC short protection with <6V clamp?
If there is no Vbus-CC short protection with <6V clamp, how to protect Vbus-CC short when we put TPD6E05U06 as ESD protection?
Regards,
kai