Part Number: SN65DP141
Other Parts Discussed in Thread: TUSB1044
Hi Sir,
I want to confirm whether sn65dp141 have a re-timer function?
I have a use case of USB3.1+DP1.2, we use a USB Type-C Cable to connect a PC(Notebook) with a AR Glass,
PC will transfer DP signal to Glass by the USB Type-C Cable and Glass will transfer UVC data stream to the PC by the USB Type-C Cable.
The USB Type-C Cable is 1.5m long and very thin, so we want use a re-timer on the cable. Just a Cable with 2 USB Type-C Port.
Does sn65dp141 can meet this feature?If not, what part of TI can meet?