Part Number: TPS25750
Hello,
I am using the TPS25750D to supply 5V out through a USB-C connector, while also being able to switch to providing 5-20V in, out to PPHV to my board.
I tried using the GUI and can't even get the flash to be programmed passed 0%.
I have my I2C lines tied to the I2Cs side and the memory tied to the I2Cm side. I have even tried to even program directly to the I2Cm lines tied to the memory.
I have tried "flashing from current configuration" and also generating a binary file and trying to file from the binary file.
All of this using the FT4232H Mini Module, which in theory should work, since it is just a USB to I2C/SPI device.
Also, the desktop version of the GUI will not open after opening the first time from install.
Any suggestions would be appreciated.
Thanks in advance