Part Number: DS90UB925Q-Q1
It is known from the specification that DS90UB925 can support YUV data.
When 925 paired with 940,If the input is YUV422-8b, I have some questions as bellow : Thanks!
1.can I connect the data bus into 925 DIN0 to DIN7 pins? Frame valid(FV) to 925 VS pin? Line valid(LV) to 925 HS pin or DE pin ?
2.How to configure 925/940 registers to work this? (I see the D/S, there no any registers Example )
See my Application as bellow:
YUV422-8b--->UB925--->UB940--->CSI(YUV422-8b)