Hi All,
I am interested in using the DP83867ERGZ-S-EVM to go from computer to independent media for transmission then use another EVM at receiver to go back to computer. The issue is I'm not sure the bandwidth capability of the independent media. Therefore, I want the capability to run 10 Mbps, 100 Mbps and up to 1 Gbps (Which I think is 1.25 Gbps with 8b/10b encoding). My concern with this EVM is I don't think it can run slower than 1.25 Gbps, I think it repeats the lower data rates to get up to that speed for transmission, is that correct? And is there a solution for my requirements, even happy to buy multiple EVMs that output at different serial speeds if need be.
Thanks for your help,
Shaun