Hi team,
I am studying fault case of TUSB211-Q1.
When resistor value for EQ setting (for example condensation of the board) is out of specified datasheet range,
which EQ level is set internally?
For example, the resistor is below?
1. < 95 ohm
2. > 105ohm and < 1710 ohm
3. > 1890 ohm and < 3861 ohm
4. > 3939 ohm and < 8645 ohm
5. > 9555 ohm
regards,