Please advice me answernig to the questions bellow.
Q1. When DS90UR906 is configured in DS90UR241 compatible mode,
which input of DS90UR241 (DIN[23:0] is corresponding to the
output of DS90UR906 (R[7:0], G[7:0], B[7:0])?
Q2. Is CONFIG0 mapped to pin #10?
Q3. DS90UR906 has MAP_SEL[1:0] pins.
The description in Taqble 11 of the datasheet is not clear to me.
Can you explain how the data is converted when MAP_Sel[1:0]
are set 00, 01, 10 and 11 respectively?
Mita