Hello,
My question is about if it is possible to split a FPD-Link III so that one video sender simultaneously can feed two video receivers. One of the receivers, called the image processing unit below, is the master of the bidirectional I2C control channel and also power provider to the sender called camera unit below. The second receiver should be able to receive video and be a slave on the I2C control channel. The splitter is preferably as "stupid" as it can be, i.e. the less computational power required for performing the split the better it is. I will not be able to output two FPD-Link III signals from the Camera unit.
Below is a figure showing, on a high level, what I want to achieve:
- Is it possible to split a FPD-Link III like I want to or is it strictly a one receiver-one sender protocol?
- If splitting is possible, is it possible to perform the split in the serial FPD-Link III domain using for example the TI DS25MB100 circuit? If possible I would like to avoid de-serializing the link, then perform the split and then serializing the data of the two split signals back to FPD-Link III again?