Team,
I have a customer that is using a TPS2052B as an input current limit switch for a 5V bus. A schematic is shown below:
The DC/DC converter that supplies the current to the TPS2052B is a 12V->5V Buck. However, it has a start up voltage overshoot as shown below:
The questions are:
1. Would the TPS2052B be damaged by this transient?
2. Would downstream devices after the TPS2052B also see the 11V spike?
Regards,
Mihir Gupta
FAE - South Germany