This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TIR1000: The requirement of 16XCLK

Expert 4255 points

Replies: 1

Views: 255

Part Number: TIR1000

Dear Team,

From the spec, it seems like we need to provide 1.843MHz clock signal to 16XCLK, but I am not sure if this clock signal is synchronous or not.

Does the clock need to synchronize with internal UART clock of the host(CPU or MCU)?

Please help to advise.

Thank you.

Jim

  • Hey Jim,

    The 16x clock does not need to be synchronous withe the UART, it is asyncronous.

    "Does the clock need to synchronize with internal UART clock of the host(CPU or MCU)?"
    -No.

    Thanks,
    -Bobby

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.