Other Parts Discussed in Thread: , LM8330, LM8333
Hi Team,
We have used TCA8418RTW to implement the keypad matrix in one of our design. The push button switches are used to connect the rows & columns.
For the EMI/EMC Certification process(IEC 61000-4-3 :80MHz to 6.0GHz at 10V/m, AM, 1kHz,80%), the board was subjected to EMC radiations. But, we are observing unintentional ghost input from TCA8418 IC, when the system is subjected to radiated susceptibility test at around 120MHz to 150MHz. huge number(Approx 5K entries) of key press events are been registered by the IC(No switch is physically pressed).
As a solution we had tried out 2 different approaches
1)Mounted ESD Diode(ESD9X3.3ST5G) on every row and Column of the IC to ground. This approach did reduce the number of key press entries registered(approx 2K entries where registered). But this couldn't resolve the issue completely.
2)Mounted 22pf capacitor on every row and Column of the IC to ground. This approach did not show any significant result compared to the one which doesn't have capacitor mounted in it.
Note:We had a switch which was not connected TCA8418 IC but connected to processor GPIO directly, We didn't find any key press event in that particular switch.This could be the reason to suspect the behavior of TCA8418.
Please suggest us a way to resolve the issue.
Regards,
Gireesh Nair