Team, please provide some guidance to my customer's question:
I am looking at adding a TI MAX3232 to my design. It requires external caps for the charge pump, denoted as C1 – C4 in the spec. I understand that for a 3.3V application, these should all be 0.1µF in value, I am pretty sure that a 10% tolerance part is fine. I need to know what voltage rating to use. Is a 16V part fine, or should I go with 25V for more margin? I think that the charge pumps develop +/- 10V. The tolerance and voltage specs for these caps are not in the TI spec.
Thanks
Viktorija