Other Parts Discussed in Thread: TCA9517, PCA9306
Hello,
Can the TCA9509 be used as an I2C repeater if VCCA = VCCB = 3.3V?
The data sheet states that both supplies can take 3.3V, so it seems like it should work as the two maximum voltages are the same:
But further on it states: “For the level translating application, the following should be true: VCCA ≤ (VCCB – 1 V)”
I’m using this as a repeater and not a translating application.
Thanks!