This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 125
Part Number: SN65LVDS33
Hi team,
My customer would like to build a SPI buffer solution with our SN65LVDS33 which has mentioned in TIDA-060017.
And, there is also a application note which is talking about SPI buffer for long distance communication as below link.
Extending the SPI bus for long-distance communication
Which one is more suggestion from your view? Which can support long transmission distance?
Thank for your kindly support.
One is a app note and the other is a reference design, you can use both for the SPI over LVDS design.
Thanks
David
In reply to David (ASIC) Liu:
Hi David,
Thanks.Customer still want to know below questions.
How do we get the delay time as below figure in TIDA-060017 such as ADS8910B, SN65LVDS33 ?
In this design, it seems doesn't mention about the delay time at host. Is there any special reason?
In reply to Feng bin Su:
Please refer to step 1 in tiducm5a design guide for the delay calculation: http://www.ti.com/lit/ug/tiducm5a/tiducm5a.pdf.