Hello,
This question is about the SN65HVD233/234/235. I have read the app note SLLA337 (Overview of 3.3V CAN Transceivers) which has a table of supply current each part draws on a 2 node CAN bus. How does the current draw scale as more nodes are added to the bus?
If both transceivers are recessive, each draws roughly 7.2mA. If both transceivers are dominant, each draws about 26mA. If one is dominant and the other is recessive, the dominant transceiver draws 38.4mA and the recessive transceiver draws 7.2mA.
If more than 2 nodes are on the bus and one transceiver is dominant while the others are recessive, what is the current drawn by the dominant transceiver? Does this value continue to scale as more nodes are added?
Why does the dominant transceiver draw a higher current when the 2nd transceiver is recessive?
Thank you