Hi team,
I feel confused about the matrix mode setting in TIC12400-Q1 datasheet. It said when using matrix polling, the wetting current CSI should be higher than CSO. If taking a 5*5 matrix as an example, does that mean the current of IN4 should be higher than IN10, IN5 should be higher than IN11, IN6 should be higher than IN12...?
But in datasheet, as shown in below picture, it set WC_CFG0[20:18] > WC_CFG0[8:6] , which means the wetting current of IN4 is lower than IN10. Is it a typo? Which one is correct? Thanks.