Hi team,
My customer is using DP83822I. Both DP83822I side and partner side are configured to Auto-negotiation mode. In normal status, if both side are configured to auto-nego, the communication speed should be negotiated to 100Mbps. So my question is:
If the environment is very bad and interferes with the communication cable, will the communication speed get degraded to 10Mbps from 100Mbps automatically? Is there any mechanism in the auto-negotiation protocal to adjust the communication speed according to signal quality when both sides are configured to auto-negotiation mode? Thanks.
Best regards,
Wayne