Hello,
I use DS110DF111 in one design. The Signal is SGMII, And I loopback Pin 24/23 (INA) with Pin 20/19 (OUTB) using a loopback board to test the Retimer. I measure the input signal on Pin 11/12 (INB) and output signal on Pin 7/8 (OUTA). The Signal on OUTA should be the same like the Signal at INB with time delay. I don't config the Retimer with I2C Bus and just use the default settings.
sometime I got signal on OUTA very quickly, sometime it takes very long time to get a signal on OUTA, sometime I can not get signal on OUTA at all. Does it mean, the input signal is not locked by the retimer? And I would like to ask, which reasons can it be and at which registers should I check (I can acess the register of retimer using I2C Bus).
Best Regards,
Lin