Hello
I am planning to use ESD122DMXR to protect cJTAG pins( MCU operation 3V) because of small size.
Please confirm we can use this or suggest dual channel smallest possible protection diodes.
Thanks,
Raghu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I am planning to use ESD122DMXR to protect cJTAG pins( MCU operation 3V) because of small size.
Please confirm we can use this or suggest dual channel smallest possible protection diodes.
Thanks,
Raghu
Hi Raghu,
The ESD122 device would be a good fit for the application. This device has a working voltage of up to 3.6V making it capable of working on the 3V line. Its low capacitance makes it capable of protecting high speed data lines without interfering with the signal integrity. The ESD122 offers IEC 6100-4-2 level 4 ESD protection, +/- 17kV contact; +/- 17kV air gap discharge, and IEC 61000-4-5 surge protection for up to 2.5A.
Let me know if you have any questions.
Best regards,
Andy Robles