This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] DS125DF410: Why my retimer is not locking? Is this related to the reference clock ?

Guru 50380 points

Replies: 1

Views: 75

Part Number: DS125DF410

When for some reason, you are not feeling well, you go to a doctor and after some questions and answers you get a prescription trying to address the immediate problem you are having. When a CDR or retimer is not achieving lock, we are the doctors and the CDR is not talking back. But we can devise different experiments to find the root cause. One of the reason could be related to a non-ideal reference clock. In this FAQ, we can test if  reference clock could be causing the device to not lock.

 

  • DS1xxDFxxx needs a stable 25MHz +/-100ppm reference clock to lock to the incoming signal. This reference clock is synthesized and enables the CDR to check incoming signal data rate. If for some reason incoming signal ppm is way off, compared to the synthesized 25MHz-clock - then it will not get qualified and CDR lock is not achieved. Given this, it is important to have a reliable reference clock. Steps below instructs the CDR to NOT use the reference clock and use a wide range of incoming signal rates to achieve lock. Given steps below, if CDR achieves lock then loss of lock is due to the reference clock.

     

    RAW   FF        0C       FF        //enable smbus write to all channel

    RAW   36       01       FF        //operate the CDR with no reference clock

    RAW   0A       1C       FF        //reset CDR

    RAW   0A       10       FF        //release reset

    RAW   02       00       00       //read CDR status. If bits 3&4 are set, CDR has achieved lock

    If we execute above steps and device is not locking then issue is not related to the reference clock.

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.