Hi Team,
Do we have RS232 which T1out and R1in pins‘ Withstand voltage could be higher than 40V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Do we have RS232 which T1out and R1in pins‘ Withstand voltage could be higher than 40V?
Hi Amelie,
Currently we do not have such a device, although high-voltage short-circuit protection can be implemented externally. An example circuit is given in the below reference design, which was developed for RS-485 but could extend to RS-232 as well:
https://www.ti.com/tool/TIDA-060027
May I ask what application would require 40 V tolerance? Is this to be able to withstand shorts to a battery voltage rail in an automotive system?
Max
Hi Max,
This is for 24V battery. The interface need to withstand 36V for 1 minute.
Thank you for the info! We'll keep cases like this in mind for future developments.
Regards,
Max