Hi team,
My customer wants to use 3.8V to supply for MAX3232E. According to datasheet, MAX3232E can operates with 3-V to 5.5-V VCC supply so I think 3.8V power supply should be OK. But I noticed that in below recommended operating condition, why there is a voltage range limitation for VCC=3.3V and VCC=5V? Can you help confirm if any voltage value from 3V~5.5V can be used to power MAX3232E? Thanks.
Best regards,
Wayne