hello TI!
I have a TUS4041 in my design and I can get it to be detected by my OS.
Here is an extract of the schematics:
The rails are up, and the PU/PD are active. GRSTz reads 3.3V.
Here is the output from the SOC console:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello TI!
I have a TUS4041 in my design and I can get it to be detected by my OS.
Here is an extract of the schematics:
The rails are up, and the PU/PD are active. GRSTz reads 3.3V.
Here is the output from the SOC console:
Hi,
Can you confirm that there is no pulldown installed on SMBUS?
Other items to check:
Regards,
JMMN
Thanks JMMN for your quick response.
Here are the answers to your questions:
Is anything connected on the downstream ports? DP will only be high if the port is populated. Are you able to see any signaling on the upstream DM line? Also, the hub may go to sleep (L2) if nothing is connected downstream.
Regards,
JMMN
Hi,
There are no devices hooked up to the USB connectors. When we try to connect a device, nothing happens.
We are going to try and use the oscilloscope on the DP/DM and try to see if there is any activity.
Still puzzled by why the device is not even recognized by the OS. Any thoughts?
Thanks!
I don't see anything obvious from the schematic. Do you see the clock start up? It may just start and stop if the hub doesn't see any signaling from the host.
Have you tried toggling GRSTz high - low - high after the system is running to see if the hub gets recognized?
Regards,
JMMN
Hi,
Thanks for your suggestions. We were trying to toggle the reset when we noticed that the device is hot to the touch.
We are thinking that the device was damaged during our debug, is that possible? We are preparing a second test board.
Thank you!
Hi,
After debug TUSB is visible, but one buggy behavior persists. If _no_ USB peripherals are connected to the TUSB4041, and you plug in a peripheral, you must manually reset GRSTZ to detect the USB device. This means the “wake” detect of the TUSB is not fully functioning, as it should detect a hot-plug in USB event normally. However, if two peripherals are plugged into ports on the TUSB, and one is removed and reinserted, the plug in event is automatically detected without having to reset GRSTZ. So as long as one peripheral is live, it behaves as expected.
Is there a setting we are missing for auto detection?
Thanks!
Hi,
This sounds like an issue on the host / driver side. Whenever there are no downstream devices connected to a hub, it is normal for a host to put the hub in suspend (low power) mode. Before it does this, however, it should configure the hub to enable remote wake. We have validated that the remote wake function works well on the hub over various operating systems, but it is possible that the Linux build is not enabling remote wake on the hub so when the connect event happen, the remote wake is not sent. Do you have any ability to configure the driver?
Regards,
JMMN