Hello,
I use a TCAN337 on a custum board with a STM32 µC. I have about 300 custums boards, and on 4 of their, I have to change the TCAN337. The RXD line is to 0V instead of 3.3V.
Have you an idea where the problem can be come ?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I use a TCAN337 on a custum board with a STM32 µC. I have about 300 custums boards, and on 4 of their, I have to change the TCAN337. The RXD line is to 0V instead of 3.3V.
Have you an idea where the problem can be come ?
Best regards.
Delmas,
Thank you for the information, it's good to know that they worked fine at some point, that may point to some kind of EOS damage. When you're disconnecting and reconnecting at CAN1 and CAN2, are the transceivers powered on?
Do you mean you have never sent any messages on the TXD pin, or you haven't tried it since they became faulty? Let me know if you can check the FAULT pin and the function of the TXD pin.
Regards,
Hello,
Yes I think the problem is EOS or ESD. Yes when I connect/disconnect CAN1 or CAN2, the transceivers are powered on. But I don't see perturbation voltage on the VDD.
I haven't any boards whit the defaut, I replace all of them. So I can't look the TXD and FAULT pin until I have an other problem.
But, how can I protect the CI for the EOS ? I have a filter and a NUP2105LT1G CI protection on the bus CAN.
Best regards.